我们今天能为您提供什么帮助?

What is the "Life" (MTTF) of ATV61/71?

Issue:
"Life" (MTTF) of ATV61/71

Product Line:
All ATV61 and ATV71

Environment:
All models and serial numbers.

Cause:
None

Resolution:
The MTTF (Mean Time To Failure) varies based on the Drive's part number. Please refer to the attached Excel sheet.

施耐德電機Taiwan

附件
MTBF for ATV 61 and 71 V 1.0.xls [898.5 KB]