我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
How many devices can the EGX 300 log?
Issue
How many power meters can EGX300 log?

Product Line
EGX300
EGX100

Environment:
Powerlogic Ethernet Gateways

Cause

1 - How many devices can an EGX300 log?
2 - How many devices can an EGX300 log if you add 1 or more EGX100s?

Resolution
1. The maximum number is 32 which is the maximum number of devices that EGX300 can connect to.

2. The maximum number is 64.

Consider both communication data and bandwidth when determining how many devices to connect to an EGX.