我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
What are the Com’X 200, Com’X 210, or Com’X 510 dimensions?
Issue
Customer is looking for dimensions for Com’X 200, Com’X 210, or Com’X 510 gateways/energy servers

Product Line
Com’X 200
Com’X 210
Com’X 510

Environment
Product dimensions.

Resolution
dimension legend
Dimensions in mm and inches