我們的品牌

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
		
我们今天能为您提供什么帮助?
EGX100 and EGX300 China Compulsory Certification
Issue
Customer needs the China Compulsory Certification for the EGX100 and EGX300

Product Line
EGX100, EGX300

Environment
EGX 100 or EGX300 is being used for the gateway

Cause
Newer certification for an older device.

Resolution
An exemption was obtained for the China Compulsory Certification since these products are at their End of Life stage. See attached documents.

施耐德電機Taiwan

附件
Signed_Contract_CCC_EGX.pdf [1 MB]
EGX100-300 for CCC exemption.pdf [127.3 KB]