我们今天能为您提供什么帮助?

What is the replacement or alternative of A9A26927 (Obsolete)?

A9A26927 was already obsoleted and replaced by either:

A9A26907 (Standard Application) - Auxiliary contact, Acti9 A9A, iSD, 1 C/O, 100mA to 6A, 24VAC to 415VAC, 24VDC to 130VDC, bottom connection

Datasheet | Instruction Sheet | CAD Files

or

A9A26917 (PLC Application) - Auxiliary contact, Acti9 A9A, iSD, 1 C/O, 2mA to 100mA, 24VAC to 250VAC, 24VDC to 220VDC, bottom connection

Datasheet | Instruction Sheet | CAD Files

For more product substitution, you may refer to the FAQ below:

Singapore: https://www.se.com/sg/en/faqs/FAQ000264549/

Malaysia: https://www.se.com/my/en/faqs/FAQ000264549/

Philippines: https://www.se.com/ph/en/faqs/FAQ000264549/