我们今天能为您提供什么帮助?

EM4800 - How to change the logging interval for energy

Issue

Customer can’t change the logging interval for Energy

Product Line

EM4000 Series

Environment

EM4800 Configuration Tool

Cause

Some customers’ applications may need to change the logging interval for Energy.

Resolution

1. Connect to the meter using the EM4800 Configuration Tool.

2. In the Report section, open the Reporting Schedule tab.

3. Change the interval setting as desired:

Reporting Schedule tab

4. Unit > Save to save the configuration.

5. Unit > Send to send changes to the meter.

Links