Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Are drive thermal output ratings available in BTU?
Issue:
Are drive thermal output ratings available in BTU?

Product Line:
All Altivar Drives, Machine, Process, Buildings

Resolution:
Heat dissipation is listed in Watts only in the Installation Manuals for the individual product.

See the drive catalog or installation manual for specific details on the heat dissipation per the exact part number.
1 watt is approximately 3.41 BTU/h
1000 BTU/h is approximately 293 W

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)