Issue:
Completely removing Vijeo Designer Windows PC Runtime
Product Line:
Vijeo Designer
Resolution:
Below are the steps to completely delete Vijeo Designer PC Runtime for Window.
You will need to unistall Vijeo Designer Runtime first.
Then delete the following:
delete C:\Program Files\Schneider Electric\Vijeo-Designer\Vijeo-Runtime
delete C:\WINDOWS\57340
delete HKEY_CURRENT_USER\Software\Schneider Electric\Vijeo-Designer Runtime
delete HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\Vijeo-Designer Runtime
delete HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Run--->RuntimeManager
delete HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\{AC7E8E45-543E-4DA9-BFFD-C140F3E3C83D}
delete HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\{DA0D2543-E9BF-4EF7-A58B-8019CEBFA84B}
If any of the files or registry keys are missing is ok, skip it and go to the next one. Once the deletion are complete, reboot the Magelis iPC or PC.
Опубліковано для: Schneider Electric Україна