Issue
Can each channel of the 140ATI03000 be configured for a different thermocouple type?
Product Line
Modicon Quantum
Environment
140ATI03000
Resolution
Yes. Each channel of the 140ATI03000 card is individually configurable. The module supports usage of types J, K, E, T, S, R, and B thermocouples.
Опубліковано для: Schneider Electric Україна