Issue
The purpose of this resolution is to inform users of the STBACO0120 analog output module that the wiring diagram is incorrect in the 'Advantys Hardware Components Reference Guide', part number 890USE17200.
Product Line
Advantys STB
STBACO0120
Environment
Resolution
The diagram in the Advantys Hardware Components Reference Guide dated 10-2006 and earlier, incorrectly shows the field device polarity for a current loop.
The following diagram correctly shows the field device polarity for a current loop.
Опубліковано для: Schneider Electric Україна