Yes the v2.0 M340 NOEs BMXNOE0100 & BMXNOE0110 do support the Network Time Protocol (NTP).
Note: Unity Pro v4.0 is required for this functionality and it is only available on the M340 NOE modules.
Опубліковано для: Schneider Electric Україна


Наші бренди
Вітаємо на веб-сайті Schneider Electric
Yes the v2.0 M340 NOEs BMXNOE0100 & BMXNOE0110 do support the Network Time Protocol (NTP).
Note: Unity Pro v4.0 is required for this functionality and it is only available on the M340 NOE modules.