Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
What is the length of the current transformer wire that ships with the Energy Meter?
Issue
The user requires the length of the current transformer wires that ship with the Energy Meter.

Product Line
Energy Meters basic (EMB) and Extended Range (EME)

Environment
Energy meter (EMB and EME)

Resolution
The length of the current transformer wires that are shipped with the Energy Meter is Six feet, 72 inches or 2 meters.