Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Meter wiring troubleshooting for Powerlogic series meters
Issue
A user would like to verify wiring on a Powerlogic series meter

Product Line
PM600 series
PM800 series
CM2000 series
CM3000 series
CM4000 series

Environment
Powerlogic series metering

Cause
It may be desirable for a user to check meter wiring for general verification or troubleshooting purposes.

Resolution
A quick check for proper readings consists of kW comparison (calculated per equation and compared to the meter reading) and a reasonable lagging 3-phase average power factor reading.
Information regarding this check, as well as further troubleshooting methods can be found in the attached "Verify_Meter_Readings" document.

If the meter values are similar to the calculated values, and are within the expected range, there is no reason to proceed with troubleshooting. If this is not true, additional phasor diagram verification will need to ensue. Reference the attached documents ("Phasor_diagram_Verification_3wire" or "Phasor_diagram_Verification_4wire") for detailed information regarding this step. The respective Phasor diagram tools required can be found attached below.

Schneider Electric Україна

Вкладення
Verify_Meter_Readings.pdf [31.89 KB]
Phasor_diagram_Verification_3wire.pdf [39.21 KB]
Phasor_diagram_Verification_4wire.pdf [19.07 KB]
Phasor_Diagram_Tool_CM3_CM4.xls [38 KB]
Phasor_Diagram_Tool_PM6_CM2.xls [27 KB]