The optional factory installed input/output module used for the portable circuit monitor is the PCMIOM-44. The PCMIOM-44 has two status inputs, one mechanical relay output, and one KYZ output.
Legacy KB System (APS) Data: RESL185155 V2.0, Originally authored by KBAdPM on 06/27/2007, Last Edited by MaTh on 10/16/2010
Related ranges: CM2000 series
Опубліковано для: Schneider Electric Україна