Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
What to do if you cannot SSH into PowerChute Network Shutdown appliance running on VMware?

Issue:
Attempting to SSH to the PowerChute Network Shutdown Appliance and receiving an error message stating that the connection has been refused.

Product Line:
PowerChute Network Shutdown Appliance for VMware

Environment:
PowerChute 4.x and 5.x VM running on a VMware ESXi host.

Cause:
SSH is not running.

Solution:
Note: All commands are in Bold Italic

Log in to the Appliance using VMware vSphere Client.

Check to see if SSH is running. The command is
systemctl status sshd

If the service is not running, run this command
systemctl start sshd

If you would like the service to start automatically with the VM, enter the command
systemctl enable sshd

When logging in as root, if the error "Access is Denied" appears, see Schneider ElectricFAQ000271236

Note: We recommend disabling SSH access when it is not required.