Issue:
Z suffix meaning on ATV61/71.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
What is the difference between the non Z suffix and Z suffix ATV61 and ATV71 drives?
Resolution:
The Z suffix means the ATV61 or ATV71 drive, will ship without the VW3A1101 graphics keypad display.
Опубліковано для: Schneider Electric Україна