Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
What is the best method on debugging a script in Vijeo Designer?
Issue:
There is no debugger for a script in Vijeo Designer?

Product Line:
scripting, Java script, Vijeo Designer

Resolution:
There is no easy way to debug a script in Vijeo Designer as the script editor does not have a debugger.  Our recommendation is to initiate a write to an internal variable to confirm the script is executing properly.