Issue:
Amp ratings for ATV212 drives.
Product Line:
ATV212, Altivar 212
Environment:
All serial numbers for ATV212 Drives
Cause:
N/A
Resolution:
The drive output ratings are available in the Installation manual.
ATV212 Installation manual is attached.
Опубліковано для: Schneider Electric Україна