Issue:
How can ATS22 be programmed for a fixed number of starts per hour?
Product Line:
Altistart ATS22
Cause:
Wants to delay the total number of times the softstarter can be started in one hour.
Resolution:
Programming:
Adj menu
Snb= number of starts Off or 1 thru 10
SLG= Start period 1 min thru 60 mins
Example= if Snb= 3 and SLG is 10 mins you can start and stop the drive 3 times in 10 mins. If you exceed the programmed start time the drive will trip out on SnbF.
***
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)
Опубліковано для: Schneider Electric Україна