Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
It is possible to detect a USB memory stick and the volume name on an LMC078?
There is no direct function or variable showing that a USB key is available or not and the related root path.  But you can use the following workaround:
FC_GetFreeDiskSpace
depending on the status value you know
0  : USB key is mounted and the device has no partition table   --> You must use ´usb2msd:0/' for the root path of the USB memory stick
-1  : USB key is mounted but the device has a partition table      --> You must use ´usb2msd:1/' for the root path of the USB memory stick
-318 : USB key not mounted