Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Where can I find wiring diagrams for the VW3A3201 and VW3A3202 ATV61/71 option cards?

Article available in these languages: Spanish

Issue:
Wiring diagrams for the VW3A3201 and VW3A3202 ATV61/71 option cards.

Product Line:
Altivar ATV61/ATV71

Environment:
All

Cause:
Needs a basic wiring diagram for the VW3A3201 and VW3A3202 option cards.

Resolution:
You can find both of the wiring diagrams in the ATV61 and ATV71 installation manuals.

wiring

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)