Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
How can you monitor the status of the ATV61/ATV71 drives remote HMI's stop button?
Issue:
Monitoring the status of the ATV61/ATV71 remote HMI's stop button.

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
How can you tell if the remote HMI's stop button has been pushed or not?

Resolution:
Address 3201 or 8603  bit 14 will show you the status of the stop button on the remote HMI

status