Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
How to detect the cable A/B status with Quantum S908 network
Background:
The manual indicates the %SW536~%SW541 as the registers to detect the cable A/B with Quantum S908 network. However, they are all zero during the test with 140CPU67160(SV3.3).

Question:
How to detect the cable A/B status with Quantum S908 network

Answer:
The feature how cpu treats system registers depends on OS version. By SV3.3, the CRP detected the cable A/B error & refreshed  its status through %SW542~%SW544