Наші бренди

Impact-Company-Logo-English Black-01-177x54

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
What would cause ground leakage current on an ATV61 or ATV71?
Issue:
What is the Ground leakage current for SCF3 fault?

Product Line:
Altivar 61, Altivar 71

Environment:
All

Cause:
Drive is tripping on SCF3 fault.

Resolution:
The threshold for a SCF3 fault (short-circuit to Ground) is 25% of drive nominal current. It is a hardware detection and it is not adjustable.