Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Can the current version of Vijeo Designer export a project saved as another older version?
Issue:
Looking for a way to save a Vijeo Designer project in an older version using the current version.

Product Line:
Vijeo Designer (all versions)

Resolution:
No, the exported VDZ file will always take the current version in which it was modified in.

ex. Vijeo Designer V6.2 will save and export to a Vijeo Designer V6.2 project.

ex. Vijeo Designer V6.2 cannot save/convert/export to a Vijeo Designer V5.0 project.