Issue
Programming software for non-Unity Quantum controllers
Product Line
Modicon Quantum
Resolution
To program Quantum non-Unity controllers you can use either the ProWORX 32 or Concept software. If you're programming in 984 ladder logic, you can use ProWORX 32 software. If you're programming in IEC languages, you will need the Concept software. Here are the ordering part numbers for the two software packages:
372SPU78001PDEV.....ProWORX 32 Offline/Online Client Software Package
372SPU47401V26.....Concept XL Software Package
These software packages can no longer be ordered through your local distributor. The software now needs to be ordered through the Service Sales group. The Service Sales group can be reached at "service.sales@schneider-electric.com". Simply give them the part number(s) and ask for pricing and availability on the ProWORX 32 and/or Concept software.
Опубліковано для: Schneider Electric Україна