Issue:
Somachine / Vijeo Designer reports Error 2897 when I build the application when I only have one device connected to COM1.
Product Line:
Vijeo Designer (all versions), SoMachine (all versions)
Resolution:
This build error occurs in Vijeo Designer when SoMachine has the "SoMachine_Network_Manager" added under COM1 of Somachine configuration.
To resolve this issue, delete the SoMachine_Network_Manager under COM1 in Somachine and the Vijeo Designer application will build properly.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Опубліковано для: Schneider Electric Україна