Issue
Is it possible to determine the actual current draw on the 'BMXCPS2000' power supply module using Unity?
Product Line
BMXCPS2000
Environment
Windows 10
Resolution
No, It is not possible to determine the actual power supply current draw on the BMXCPS2000 M580 power supply module.
Is it possible to determine the actual current draw on the 'BMXCPS2000' power supply module using Unity?
Product Line
BMXCPS2000
Environment
Windows 10
Resolution
No, It is not possible to determine the actual power supply current draw on the BMXCPS2000 M580 power supply module.
Опубліковано для: Schneider Electric Україна