| Issue: How can I check the fault history in the ATV32 drive? Product Line: ATV32, Altivar 32 Environment: All part numbers, all models Cause: Customer wanted to know if drive has a fault. Resolution: The fault history is in the Diagnostics menu, and can be accessed using the graphics keypad VW3A1101, or SoMove software. |
Опубліковано для: Schneider Electric Україна