Наші бренди

Impact-Company-Logo-English Black-01-177x54

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Is the Smoke Purge option Available on ATV660 Enclosed Drives?
Issue:
​Smoke Purge option on ATV660 Enclosed Drives.

Product Line:
ATV660, Altivar 660

Environment:
All

Cause:
Smoke Purge option is not listed in Catalog

Resolution:
The Smoke Purge is available as an Engineered To Order (ETO) option for the time being.  See your local distributor or Area Drives Manger for details.