Issue:
"EU" suffix on a ATV630 drive
Product Line:
Altivar Process Drive
Environment:
ATV630/ATV930
Cause:
EU Suffix
Resolution:
EU indicates the drive is rated for IP55 (Nema 12) and includes a disconnect switch.
"EU" suffix on a ATV630 drive
Product Line:
Altivar Process Drive
Environment:
ATV630/ATV930
Cause:
EU Suffix
Resolution:
EU indicates the drive is rated for IP55 (Nema 12) and includes a disconnect switch.
Опубліковано для: Schneider Electric Україна