Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
What is the part number for the ATV630 Flange mounting kit?

Issue:
Flange mounting kit part number for ATV630.

Product line:
ATV630, Altivar Process

Environment:
All models.

Resolution:
The flange mount kit is based on the ATV630 part number.  See the following spreadsheet for selection.

See attachment

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

Schneider Electric Україна

Вкладення
FA299185.jpg [107.38 KB]