Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Benefits of utilizing Altivar 680/980 Series Variable Frequency Drives?

Issue:
Benefits to the reducing noise voltages with the ATV680/980 drives.

Product Line:
ATV680 ATV980

Environment:
All

Cause:
Benefits of voltage noise

Resolution:
The connection of DC-voltage midpoint with artificial star-point built by filter capacitors will reduce the bearing currents, increase the lifetime of motor bearings and allows for easy paralleling of power stages.