Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Inverting CT polarity on EM4000 / EM4800 / E4800 using EM4800 Configuration Tool

Issue
The EM4000 / EM4800 / E4800 is reading incorrectly due to an inverted CT. The customer is not able to physically invert the CT; however he/she would like the meter to read correctly.

Environment
EM4800 Configuration Tool

Resolution
To invert the CT polarity via the EM4800 Configuration Tool, place a negative sign in front of the CT primary value. An example is shown below:

If the CT ratio is 600:5, the Current value should be changed from 600 to -600.
Figure1 Figure 2

The EM4800 Configuration Tool if available for download