Чим ми можемо вам допомогти сьогодні?

Video: How can one unlock the ATV630/930 drive's display to access menus and parameters?

Article available in these languages:

  • Finnish

Issue:
Wanted to unlock the ATV630/930 drive's display to access menus and parameters.

Product Line:
Altivar Process 630 & 930

Resolution:
Press and hold the home button and ESC button together for 2 seconds.
You can also choose to disable this function by going into [My preferences]-> [LCD settings]-> [Display terminal locked] and set that parameter to 'NO'.