Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Video: How to setup a fault reset function on an ATV212 drive?
Issue:
ATV212 set up a fault reset function.

Product Line:
Altivar 212

Resolution:
RES terminal on the ATV212 which is parameter F113 is already programmed as fault reset from the factory.
F113 under F--- set to 10 for fault reset.
When RES is has +24VDC present on terminal that will perform a fault reset.

Warning:
UNINTENDED EQUIPMENT OPERATION
This configuration enables to reset the drive.  Make sure that this action will not endanger personnel or equipment in anyway.

Reminder that not all detected faults can be cleared.  Please check your ATV212 programming manual for a list of the faults that can be cleared using the fault reset function.