Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Can you adjust the motor speed with an ATS48 or ATS22 soft starters?
Issue:
Wants to adjust the motor speed with an ATS48 or ATS22 soft starters.

Product Line:
Altistart 22, Altistart 48, ATS22, ATS48

Environment:
All

Cause:
Soft starters do not have IGBTs which gate voltage/ frequency to the motor, allowing for different speeds or frequencies.

Resolution:
The soft starter will only ramp up voltage at 60 hz.   There is no option for speed control using a soft starter.