Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Is it possible in Unity pro to force %IW values directly from the Animation Table with M580?
Issue
Need to force analog input DDT in the M580.

Product line
M580, Unity pro , Control Expert

Resolution
It is possible now to force Analog inputs on M580 with unlocated data model (on Device DDT).
it will not be implemented on located data, because Schneider focus is on unlocated Data with M580.