Issue
What are the specification for the fiber optic communication with the ION8650 meter?
Product Line
ION8650
Environment
Fiber optic communication
Resolution
The part used for fiber optic communication is AFBR-5803AQZ from Broadcom Link to site.
| Connector Type | SC |
| Data Rate | 125 MBd |
| Emitter | LED |
| Fiber Type | Multimode Glass |
| Maximum Distance (m) | 2000 |
| Nominal Optical Wavelength (nm) | 1300 |
Опубліковано для: Schneider Electric Україна