Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
On an ATV12, why can't SoMove be connected with a standard Cat 5?
Issue:
ATV12 SoMove connection with standard Cat 5

Product Line:
ATV12

Environment:
All

Cause:
Wiring

Resolution:
There is no Ehternet Port and no option for Ethernet on the ATV12 drive. SoMove software, the DTM's and updates are found free online at http://www.altivardrives.com/3; however, you have to connect using the TCSMCNAM3M002P.