Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Can you use a Servo stepper motor on the ATV600 and ATV900 Process drives?
Issue:
ATV600 and ATV900 process drive running a servo stepper motor.

Product Line:
ATV600 and ATV900 Process drives

Environment:
All

Cause:
Wants to run a stepper motor on the ATV960 drive.

Resolution:
No you can not run a stepper motor on the ATV600 and ATV900 process drives.  You will need to look a the Servo Lexium drive.