Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Is the 2510F manual starter acceptable to OSHA as an energy isolation device suitable for lockout / tagout?
Issue:
2510F manual starter acceptable to OSHA as an energy isolation device suitable for lockout / tagout.

Product Line:
2510 Type F

Environment:
All models

Cause:
N/A

Resolution:
These do not meet OSHA requirements for Lock Out/Tag Out. This product is a manual starter, not a disconnecting means.