Issue :
Adjust language of the drive.
Product Line :
Altivar Process Drive, ATV630, ATV930
Resolution :
The drive's default language is in English. Yet in some cases during programming, the language is changed. Below are the steps to revert the drive's language to English:
- Push the Home and Escape button at the same time to make sure the display is unlocked
- Push Home button, to get back to the Main Display
- Scroll down to the bottom the last parameter in the list. This should be Menu 8 - My Preferences
- Push the OK button (Menu 8.1 Language)
- Push the OK button a second time. This takes you into the language options
- English is at the top of the list
- Push the OK button on English to save the setting
These settings can be found in the ATV Process drive Programming Manual under Chapter 10, My Preferences.
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
Опубліковано для: Schneider Electric Україна