Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Video: How to change a password on AccuSine PCS+
Issue
Modifying the password of an existing user of AccuSine PCS+ via the display.

Product Line
AccuSine PCS+

Environment
HMI

Resolution


Please follow the steps below to change the password of an existing user:
  1. Press "User Login"
  2. Log in with the user name and existing password
  3. Press Change Password
  4. Enter the new password
    • The password must be between 6 and 32 characters with any combination of letters or numbers. Passwords are case sensitive.
  5. ​Re-enter the new password in the "Confirm" field
  6. Press "Change Password"
  7. Keep password in a secure location so it is not lost