ATS01, ATS130 has very simple logic for limiting starting current and so there are no exact values of starting time. The starting ramps are not fully controlled like in ATS22 or ATS480.
See attached resolution to know the influence of setting on starting current and time. Although it was written for ATS01, it is applicable for ATS130 as well.
Опубліковано для: Schneider Electric Україна