Наші бренди

Impact-Company-Logo-English Black-01-177x54

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Is the XVUZ12 the same as the XVBC12?
Issue:
What is difference between XVBC12 and XVUZ12?

Product Line:
XVB and XVU Tower lights and beacons

Environment:
Tower Lights and Beacons

Resolution:
The XVUZ12 is the wall mount bracket or fixing plate for use on vertical support for the XVU series. The XVBC12 has the same function for the XVB series. The center hole on the XVBC12 is round shape, the XVU is oblong shape. The two lines of Tower Lights are not interchangeable.
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
  • Знайти наші представництва"