Наші бренди

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Is the P24 and 24V the same on Altivar Process Drives?
Issue:
Difference between the P24 and 24V supplies on Altivar Process Drives

Product Line:
ATV6xx   ATV9xx

Environment:
All serial numbers

Cause:
P24 voltage rating

Resolution:
Yes, there is a difference.
P24 is a +24Vdc external input supply maximum current: 0.8 A
24V is a +24Vdc output supply for digital and STO safety inputs: maximum 200 mA

+24
P24