Чим ми можемо вам допомогти сьогодні?

Is it possible to having FTP data publishing more frequent that 1 hour on the COM’X 510?

Issue
Is it possible to having FTP data publishing more frequent that 1 hour on the COM’X 510?

Product Line
COM’X510

Environment
FTP Data Pushing

Cause
The maximum default option for FTP data publishing interval is 1hour, but a shorter interval is needed.

Resolution
There is no a way to publish more frequently than once an hour. The available Publication frequency are: Every hour, Every 2 hours, Every 3 hours Every 4 hours, Every 12 hours, Every day, Every week, and Every month.