Наші бренди

Impact-Company-Logo-English Black-01-177x54

Вітаємо на веб-сайті Schneider Electric

Ласкаво просимо на наш веб-сайт.
		
Чим ми можемо вам допомогти сьогодні?
Video : How to Install Firmware in a 170ENT11001 Ethernet Adapter
This video describes the procedure to install the firmware and web page files to a 170ENT11001 Ethernet Adapter that are with Momentum IO bases.

These instructions pertain to the RoHs version Ethernet Communication Adapters only.  Since the part number is the same for both a RoHs and non-RoHs communication adapter, a RoHs compliant 170ENT11001 is identified by adapters laser marked with an SV at v1.10 or higher.  Non-Rohs versions will always have an Exec version less than 1.10.  There are no other physical differences between the two adapters.