Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is happening if the Sphere Wireless Lighting System seems to change by itself?

**Please Note: The Sphere range of products are no longer available in the UK**

Sphere control commands are heavily encrypted. As such unexpected changes to the lighting in one or more rooms can only be caused by Sphere Controllers that have the same switch settings being operated nearby, for instance in adjacent rooms or neighbouring apartments that have the Sphere system. However it is still possible that interference could occur if a new Sphere system is installed locally. In this case, the House switch settings on the Controller of the affected room(s) will need altering.

Schneider Electric UK
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
  • Help and contact centre